Technical FAQs

Ask a Question

Filter results

Clear
What are the differences between the Back-UPS RS and the Back-UPS XS models (Does not Include BX/BR LCD Models)
Issue: What are the primary differences between the Back-UPS RS and the Back-UPS XS models (Does not Include BX/BR "LCD" or BX/BR "G" Models) Product...
How can I adjust the number of battery packs on a Smart-UPS XL?
Issue: Smart-UPS XL products require that you tell the UPS how many external batteries are connected so that the UPS can properly calculate runtime....
What is the battery type and technology used in APC UPS Systems?
Issue: What is the battery type and technology used in APC UPS Systems? Product Line: All APC Single Phase UPS Battery systems. Environment: All APC...
What is Peak Surge Current rating?
Issue: What is Peak Surge Current rating? Product Line: All APC  Surge and Back-UPS products. Environment: All APC Surge and Back-UPS products. Cause...
PowerChute Personal Edition systray icon missing in Windows XP
The Windows XP task bar has an option to hide unused icons. This option in Windows is enabled by default. Therefore, icons that have not been used...
How do I upgrade my SRT or XP Smart-UPS firmware using my Network Management Card?
Issue What are the steps in order to use my Network Management Card to update my Smart UPS (SRT) or Secure-UPS (XP) firmware?   Product Line   Smart-UPS...
Configuring Post-only Mode for Netbotz Version 2 and 3 Appliances
Issue: Configuring Post-only Mode for Netbotz Appliances Product Line: NetBotz. Environment: NetBotz version 2 and 3 NetBotz Central 2.x InfraStruxure...
Where are your TechCool manuals?
Issue: Where are your TechCool manuals?   Product line: Airflow TechCool Units   Environment: Data Center Cooling   Cause:   Resolution: The TechCool...
Why is my ACRP excessively cycling?
Issue: Why is my ACRP excessively cycling?   Product line: ACRD50x, ACRp10x   Environment: Data Center Cooling   Cause:   Resolution: Most refrigeration...
Details Returned from Best Power Devices via Advanced Device Crawlers
Issue: Details Returned from Best Power Devices via Advanced Device Crawlers Product Line: NetBotz Environment: NetBotz version 2 Advanced Device...
Results 11 - 20 of 100