Technical FAQs

Ask a Question

With Hyper-V support enabled, PowerChute Network Shutdown is slow loading some UI pages and PowerChute Hyper-V Powershell scripts take longer than expected to execute.
Issue: On a Hyper-V system, PowerChute Network Shutdown is slow in the instances mentioned: a) when displaying some user interface pages b) in running...
How do software support contracts work for StruxureWare Data Center Expert.
Issue: How do software support contracts work for StruxureWare Data Center Expert. Product Line: InfraStruxure Central StruxueWare Data Center Expert....
EcoAisle Rail Mounting Bracket Submittal
                                                                                                                                                 ...
Uniflair Pump Packages Technical Specs
Issue: Uniflair Pump Packages Technical Specs Product line: Uniflair Environment: Data Center Cooling Cause: Product Design Specifications Resolution:...
What should be checked if the NetShelter CX internal temperature exceeds expected levels? (5*C/41*F above room temp)
Issue: Excessive temperature in NetShelter CX. Product Line: NetShelter CX   Environment: All versions and serial ranges.   Cause: Fan issues, air...
PowerChute Network Shutdown v3.1 cannot connect to vCenter Server or ESXi hosts to perform VM and host tasks
Issue: PowerChute Network Shutdown connects to vCenter Server/ ESXi Host Web Services using the URL "https:///sdk" using TCP port 443....
Why does PowerChute Network Shutdown not establish communications with Network Management Card when Radius is enabled?
Issue: PowerChute Network Shutdown will not establish communications with Network Management Card when Radius is enabled. Product Line/s: PowerChute...
Will the NetShelter CX fit through standard doors?
Issue: Will the CX fit through a standard door opening? Product Line: NetShelter CX   Environment: All versions and serial ranges.   Cause: Need to...
How deep must the AR7580A Cable Manager be installed so the AR7581A Hinged Cover can open 90 degrees?
Issue: Need to make sure the cable cover opens far enough to install and maintain cables. Product Line: NetShelter SX   Environment: All versions...
PowerChute Network Shutdown v3.1 & 4.0 Required VMware vSphere Permissions
ISSUE: What vSphere permissions are required by PowerChute Network Shutdown v3.1 for VMware? Product Line: PowerChute Network Shutdown v3.1 & 4.0...
Results 11 - 20 of 100