Technical FAQs

Ask a Question

Filter results

Clear
Using Zentyal Linux FreeRADIUS along with APC Network Management Card Devices
Issue Using Zentyal Linux FreeRADIUS along with APC Network Management Card Devices Product Line Network Management Card 1 - AP9617, AP9618, AP9619...
DNS may not work properly after firmware upgrade on Network Management Card 1 (NMC1) when using DHCP boot mode
Issue After a firmware upgrade, DNS may not work properly until DNS server settings are re-applied in some fashion, specifically when the Network...
Why is my Network Management Card's default gateway showing as 0.0.0.0 under Current IPv4 settings?
Issue Within the Network Management Card web interface, why is my default gateway showing as 0.0.0.0 even though I entered a gateway? See below for...
AOS v6.3.2/sy3p APP v6.3.2 UPS Network Management Card 2 (NMC2) AP9630/AP9631 UPS Compatibility
Issue This knowledge base will specify the compatibility of UPS Network Management Card 2 (NMC2) AP9630/31 sy3p APP v6.3.2 compatibility. Product...
Network Management Card 2 (NMC2) - SNMPv1/v3 walk beginning at .iso through .iso.org.dod.internet does not work properly
Issue An SNMPv1/v3 walk beginning at .iso through .iso.org.dod.internet does not work properly with my Network Management Card 2 device. If a user...
Why doesn't the web interface of my APC Network Management Card finish loading?
Issue The web UI of my Network Management Card does not load completely. For example, minor image parts may not load, such as corners of the tabs...
UPS Network Management Card 2 Firmware Application Compatibility for Smart-UPS Online (SRT) Models
Issue Which UPS Network Management Card 2 (NMC2) firmware applications work with my SRT model UPS? Users experiencing NMC2->UPS communication problems,...
"On Battery" status when using Isolated Extension Cable (Part # AP9825)
Issue "On Battery" status when using Isolated Extension Cable Product Line   Interface Cables Isolated Extension Cable (IEC) - AP9825 Environment...
"Received ssh2_msg_channel_success for nonexistent channel 65536" error message using SSH with PuTTy v0.63 and higher with APC Network Management Card 1 (NMC1) devices
Issue A user may receive the following error message when using newer versions of PuTTy SSH client with NMC1 devices: "disconnected: received ssh2_msg_channel_success...
50A 208v 3 Phase Rack PDU Load Ratings and Calculations Explained
Issue 50A 208v 3 Phase Rack PDU Load Ratings and Calculations Explained Product Line 3 Phase Rack Power Distribution models AP84XX AP86XX AP88XX AP89XX...
Results 11 - 20 of 27