{}

Our Brands

Search FAQs

PowerChute Network Shutdown versions 4.x Required VMware vSphere Permissions

ISSUE:
What vSphere permissions are required by PowerChute Network Shutdown 4.x for VMware?

Product Line:
PowerChute Network Shutdown versions 4.x for VMware

Environment:
vCenter Server 5.x, 6.x, 7.0
ESXi 5.x, 6.x, 7.0

Cause:
Permissions required by PowerChute Network Shutdown when performing VMware related functions.

Resolution:

The attached PDF outlines the permissions required by PowerChute Network Shutdown to carry out the tasks below:
Deploying PowerChute Virtual Appliance
Creating the vCenter Plug-in
Creating and triggering vCenter Alarms
Virtual Machine Migration
Virtual Machine Shutdown/Startup
vApp Shutdown/Start
Putting Hosts in to maintenance mode
Shutting down Hosts
This allows you to create a service account role for PowerChute in vSphere instead of assigning the Administrator role which has full privileges.

APC USA

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.