White Papers

:
-or-
:
-or-
:
-or-
:

1 result(s) found.
Number Title & Abstract
Pdf
WP-62 v1
Powering Single-Corded Equipment in a Dual Path Environment
The use of dual power path architecture in combination with IT equipment with dual power supplies and power cords is an industry best-practice. In facilities using this approach there are inevitably some IT devices which have only a single power cord. There are a number of options for integrating single-corded devices into a high availability dual path data center. This paper explains the differences between the various options and provides a guide to selecting the appropriate approach.