Search FAQs
What's the difference between shipping load, dynamic load and static load? Which standards are used to certify these ratings?
Issue:
Shipping, moving and loading cabinets requires the installer to know the difference between shipping load, dynamic load and static load ratings.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Installers and designers need to make sure the load capacity of the cabinet is not exceeded during installation, travel or operation.
Resolution:
Please see attachment for load ratings, definitions and standards.
Shipping, moving and loading cabinets requires the installer to know the difference between shipping load, dynamic load and static load ratings.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Installers and designers need to make sure the load capacity of the cabinet is not exceeded during installation, travel or operation.
Resolution:
Please see attachment for load ratings, definitions and standards.
Released for:APC United Kingdom
Attachment(s)
Explore more