Browse FAQs



Oil Type for Different Types of Refrigerant
R134A Use POE oil Units : RDU but no oil needed for this unit on startup.
Can you interconnect A-Links CW and DX InRow Cooling products?
1 ) Cannot ... Just to clarify, it's "like" units , so 600mm DX with other 600mm DX; and 600mm CW with other 600mm CW; however, 600mm CW and 600mm DX can NOT be grouped, even though they share the same FW. ... Pumped Refrigerant Cooling System (PRCS, r134a ...) ... For 300mm Units and Pumped Refrigerant :
Installation Manual for the acda901
acda901, RDU , install manual, installation, manuals, pumped refrigerant
Refrigerant charging table for a Uniflair Unit
Refrigerant charging table for a Uniflair Unit . ... -cooled DX units must be connected ... Install all refrigerant lines in accordance ... • All refrigerant piping is type ... • All refrigerant lines/chilled ... • All refrigerant lines should be ... • All refrigerant piping joints must ... • All refrigerant pipes are installed ... supports and approved refrigerant line clamps. ... lines and the refrigerant connections must be ... ... sized such that refrigerant velocity in vertical ... Refrigerant velocity in horizontal ... Refrigerant velocity must be ... If refrigerant velocity is too ... If the refrigerant velocity is too ... ... to ensure sufficient refrigerant flow to the ...
Liquid Charging an InRow 600mm Refrigerant Based System
... an InRow 600mm Refrigerant Based System ... , discharge and service port when evacuating ... 1 ) Close the ... ... to the corresponding service ports on the ... ... with the vacuum pump . ... pressure sides and service port (rp10x ... activate the vacuum pump . ... .. Indoor Unit Charge + Liquid ... 7) Charge with liquid, preferably at the outdoor receiver, until the system pressure equalizes with the refrigerant canister. a. Apply the charge into the service port (rp10x & rd50x) on the equipment service bracket. b. Purge the refrigerant hoses and manifold set.
How to navigate through an Network Air FM unit display
Refrigerant . ... the type of refrigerant charge used in ... ... out into the refrigerant line. ... out into the refrigerant line. ... and then keeps coolant flowing through the ... ... compressor (stage 1 ) in a ... ... is adequate liquid coolant (glycol or ... ... switch detects inadequate coolant flow at the ... ... the flow of coolant into the heat ... ... the flow of coolant to either the ... ... to a common coolant source, coolant flow through a ... ... The Economizer ( coolant ) isolation valve ... instances to stop coolant flow through a ... a variable speed coolant pump is used.
Where can I get support for APC and MGE Products?
Assessment Services ... Battery Replacement Services ... Cabinet Power Distribution ... Configurable Power Distribution ... Data Distribution Cable ... DC Distribution Components ... Environmental Monitoring Unit ... InRow Pumped Refrigerant Installation Services ... MGE Service Bypass ... Modular Power Distribution ... Network Integration Services ... On Site Service ... Power Distribution Units ... Project Management Services ... Refrigerant Distribution Remote Monitoring Services ... Service Bypass Panel Service Plans ... Start-Up Service Stationary Power Distribution Units ... Training Services
DAC, Cancoil Installation Manual
Section 1 . Warranty and ... Section 1 . ... provided in the unit . DO ... SECTION OF THE UNIT . ... not use the refrigerant piping as a ... Unit Placement and Mounting ... unit should be securely ... ... clearance around the unit for proper servicing and preventative maintenance ... ... are based on 1 degree per 100 ... ... a rate of 1 ” drop per ... ... a rate of 1 ” drop per ... ... and should have 1 additional trap per ... ... , however many units are shipped without ... . Check the unit wiring diagram for ... ... venting of harmful refrigerants to the ... A mixture of refrigerant (35 PSIG ...
InRow RC Standard and Optional Features
1 -The Standard Features of the InRow Rc Coolling Unit are as follow: ... Condensate Pump with Dual Float Switches ... Power Trough (Overhead power distribution between racks)


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.