Uniflair Manual Start Up and Shut Down (PCO1)
... Start Up the Unit ... . Unlock the main switch. ... all of the circuit breakers on the ... ... and all system pipes have been bled ... 7. For internal pipe , it is necessary to remove the frontal security metal sheet. ... If an alarm is indicated, consult the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual. Turn Off the Unit 1. On the first user interface screen, press the UP or DOWN buttons until the SWITCH OFF UNIT screen appears. ... For additional information, see the Uniflair Chilled Water and Direct Expansion Operation and Maintenance manual.