Rack PDU 2G (AP8XXX) Network Port Sharing Information
... ability to share one IP address via one network connection) ... status of and configure and manage up ... PDUs using only one ... a number, 1 to 4, ... ... are connected to one another in a ... ... selecting the Display Settings > Display ID ... ... " port of one of the grouped ... ... the Establish Network Settings section. ... desired order, 1 to 4. ... ... have Display ID 1 . ... ID can be configured from the the ... the "Device Manager > Load Management ... ... viewing status and configuration /control. ... (AOS) module and the application module .