Browse FAQs



Video: How do I upgrade my SMT/SMX Smart-UPS firmware using my Network Management Card?
... update my Smart UPS (SMT/ ... Smart- UPS models with the ... Supported UPS model listed above UPS Network Management Card ... UPS power output * ... ... for the particular UPS (Links are ... UPS Firmware Updates allow ... ... recommend using the APC Firmware Upgrade Wizard ... connection to the UPS whenever possible. The APC Firmware Upgrade Wizard ... ... their Smart- UPS Firmware using an APC Network Management Card ... ... and update the UPS via the Network ... ... Find the correct UPS Firmware Image. Use the UPS "ID" ... Image for your UPS . ... platform of your UPS .
Why is the UPS thermal dissipation rating calculated using efficiency data different from the value specified on www.apc.com?
The thermal dissipation rating specified on the APC website is sometimes different than the value calculated using efficiency data or the UPS Efficiency Comparison Calculator. ... The value calculated using efficiency data or the Efficiency Comparison Calculator is based on nominal environmental conditions (25C, 230v 50hz input), in green mode with a fully charged battery. The values on the web are specified for less-than-nominal environmental conditions, such as maximum charging power, active AVR , high ambient temperature, etc.
What are the features of the switched outlet groups on my SMT, SMX, or SRT Smart-UPS?
... Generation Smart- UPS have switchable outlet groups which can ... Smart- UPS , Smart- UPS Online ... All Smart- UPS SMT, SMX ... to turn their outlets on and off ... ... two types of outlet groups: Main Outlet Group ... output of the outlets on the UPS Switched Outlet Group ... A group of outlets that functions as ... of the Main Outlet Group. The Main Outlet Group must be ... of the Switched Outlet Groups to be ... ... Some models feature outlets in addition to ... Only the outlets are switched.
Why would I need to use the 24VDC adapter when using the APC Isolated Extension Cable?
When attempting to connect a system running PowerChute plus in simple signaling through an Isolated Extension Cable ( IEC ), you must use a 24VDC adapter to power the UPS End Unit of the IEC . ... This adapter is available for purchase on APC's Web site (www.apcc.com). Users may also find an equivalent power adapter at their nearest electronics store .
Frequently Asked Questions for the new SMX and SMT series of Smart-UPS products.
... of Smart- UPS products. Smart- UPS SMT and SMX ... of Smart- UPS is an all ... of Smart- UPS product with many ... UPS Frequently Asked Questions ... management and monitoring easier APC’s patent pending ‘ ... voltage regulation ( AVR ) when not ... AVR is typically handled in the line interactive design by solid state transformers. ... Why do the new UPS’s not have a DB9 serial port? ... New Smart- UPS models utilize PowerChute Business Edition version 8.5 or later only. ... We recognize the fact that some Smart- UPS customers utilize their own custom interface based on APC’s UPSLINK protocol. ... UPS UPS UPS ... UPS
Do I need to use a 24VDC power adapter with the Isolated Extension Cable?
When attempting to connect a system running PowerChute in simple signaling through an Isolated Extension Cable ( IEC ), you must use a 24VDC adapter to power the UPS End Unit of the IEC . ... This adapter is available for purchase on APC's Web site (www.apcc.com). ... Users may also find an equivalent power adapter at their nearest electronics store .
Battery Discharge During Storage
... life of a UPS battery under storage ... All UPS products ... life of a UPS battery under storage ... For each APC UPS family the expected ... ... used in all UPS products has a ... ... Back-UPS AVR , Back- ... , Smart- UPS v/s ... any of these APC UPS models has been ... ... With Smart- UPS ... a Smart- UPS . ... , if the UPS is switched off ... ... , if the UPS is switched off ... ... order for the UPS to "remember ... ... hours if the UPS is not operating ... ... With Matrix- UPS ... a Matrix- UPS .
What is AVR (Automatic Voltage Regulation)?
Product Line: Line-R, Back-UPS, Back-UPS PRO, Smart- UPS and APC AV.
What is the expected life of my APC UPS battery?
Do not store APC batteries for extended periods of time.
Using the 940-1524 Smart Signaling Cable and UPS Interface Extension Cables
The Network Enhancements division has developed an Isolated Extension Cable ( IEC ), APC part number AP9825 which converts serial RS-232 signaling ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.