Browse FAQs

Galaxy VS; Why is FTP being logged in the event log but no external cause for logging FTP found?

Published date: 25 February 2020

Issue:
FTP is being logged in the event log but no external cause for logging FTP


Product line:
Galaxy VS


Environment:
Galaxy VS


Cause:
Bug in the current firmware 4.28.  Some UPS to NMC communications like Waveform generation are being logged by the NMC.  FTP events should be communications between NMC and external applications such as EcoStruXure IT or DCE.


Resolution:
Next firmware release should resolve this logging anomaly.
 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.