Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
Cause: StruxureWare Data Center Expert appliances come with 2 years of factory hardware warranty and no
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
1 . Open the application 2. Enter IP address or hostname within the "Host Name" field
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
The StruxureWare Data Center Expert Desktop Client (console) is a stand -alone Java application that runs on systems that meet the following ...
Data Center Expert | How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
1 ) Navigate to ... Installation directory for StruxureWare Data Center Expert. ( ... C:\ Program Files (x86)\ StruxureWare Data Center Expert X. ...
NetBotz Rack Access does not discover when choosing NetBotz discovery in StruxureWare Data Center Expert (DCE)
300, 400, and 500 series NetBotz appliances, it must be discovered as an SNMP device in StruxureWare DCE.
Why does ISX Manager/StruxureWare Central display the incorrect Kilowatt value when utilizing the Physical Layout or ISX Operations feature for my Metered/Switched Rack PDU product?
... or ISX/ StruxureWare Operations tools from my Metered or Switched Rack PDU. ISX Operations StruxureWare Data Center Operations ... and AP88XX Metered Rack PDUs ... Metered By Outlet Rack PDUs ... and AP86XX Metered Rack PDUs ISX or StruxureWare Operations - All Versions ... Physical Layout or StruxureWare Central Operations to display the ... ... (AP79XX) Rack PDU's as well ... ISX Manager or StruxureWare Central via SNMP ... Physical Layout or StruxureWare Operations tool. The problem that occurs stems from the Metered/or Switched Rack PDU and inline current meters reporting incorrect voltage. ... Alternatively, these values can be changed via SNMP on most prior rpdu APP revisions.
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not ... StruxureWare Data Center Expert (DCE ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all ... StruxureWare Central (all ... SturuxureWare Data Center Expert requires a ... passcode and the Data Center Expert's MAC address ... StruxureWare Data Center Expert (DCE ... ... to gather specific information about the alert ... 1 . In a ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine SFDCOBASE = StruxureWare Data Center Operation ... a VM or Data Center Operation .
Why isn't my DNS change saving in StruxureWare Data Center Expert?
Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes. ... StruxureWare Data Center Expert ... StruxureWare Data Center Expert VM with single NIC configured ... It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers, only on a DCE VM server.
File transfers may be unsuccessful using SCP on devices within StruxureWare Data Center Expert (DCE) with v6.X.X firmware earlier than v6.3.3
... using SCP within StruxureWare Data Center Expert may be ... ... NMC2 such as Rack PDU StruxureWare Data Center Expert ... the device through StruxureWare Data Center Expert, you ... ... enabled devices and applications . You can do this within StruxureWare under the Updates->Apply Firmware Updates screen within the DCE client. ... If using StruxureWare DCE for this configuration, make sure to set the correct "Device File Transfer Settings” options in DCE before you select the v6.X.X devices you want to update.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.