Browse FAQs



AP84XX, AP88XX, AP89XX, and AP86XX 2G Rack PDU LCD Backlight Behavior
Rack Power Distribution ... backlight on the PDU will be illuminated blue all of the ... ... span of the rack LCD display and ... ... remain on for 10 minutes. Then, 10 minutes after the ... ... PDUs or each PDU in a Network ... ... Metering by Outlet Rack PDUs require v ... ... display of the PDU under Main Menu ... Within the network management card web interface ( blue and white), please check under Administration->General->About and note your AOS and rpdu2g APP versions.
Network Management Card (NMC) Password Reset Procedure
... : Environmental Monitoring Unit 1 (AP9312TH ... ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... , Environmental Monitoring Units (ap9320, ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... Rack PDU (AP84XX* ... 1st Generation Rack Automatic Transfer Switch ... 2nd Generation Rack Automatic Transfer Switch ... 4th Generation Rack Automatic Transfer Switch ... Rack Air Removal Unit (acf400, ... Rack PDU 1G and ... 1st Generation Rack Automatic Transfer Switch ... 2nd Generation Rack Automatic Transfer Switch ... 4th Generation Rack Automatic Transfer Switch ...
Rack PDU 2G (AP8XXX) Network Port Sharing Information
Updating firmware for Network Port Sharing Groups ... , check that the total length of network cable between up to four units is not more than 10 meters.
After upgrading firmware on my APC AP8XXX series Rack PDU, the input voltage reads 1V
... reason, APC Rack PDU engineering has been ... load on the Rack PDU , reducing the ... cycling the entire Rack PDU for 5- 10 seconds.
APC Switched Rack PDUs - any pending outlet commands are lost when PDU Network Management Interface is rebooted
Do not power the Rack PDU's network connection by the same Rack PDU's outlets (and turn ... off for longer than 10 minutes) -
Why is my AP561X KVM Switch Not Recognizing My Rack PDU for Power Management Integration?
... an APC Switched Rack PDU beginning with AP79XX ... KVM Switch's port labeled ' PDU ,' ' ... a supported Switched Rack PDU is the required ...
About->Support menu option missing from AP8XXX series Rack PDU Web Interface on certain firmware versions
like this: http:// 10 .10.10.10/NMC/secmwbb5rt0tyowdufibga/gentrbl.htm
Why are the red outlet LEDs always scrolling on Rack PDU models AP7855 or AP7867?
It will prompt the user to enter the load value. Enter the load value in multiple of 10 (ex.
50a 208v 3 Phase Rack PDU Load Ratings and Calculations Explained
Why is AP8868 rated at 10 .0kw, when AP7868 was rated at 12.5kw? allows for short-term headroom for any power spikes that may occur. Best practice should have allowed for this headroom, even on the previous generation of products. The internal circuit breakers are the same type - 20a, UL489, branch rated, and hydraulic magnetic. The pictures


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.