Browse FAQs



INFORMATION BULLETIN: Potential Issue with AP8XXX series Rack Power Distribution Units with rpdu2g v6.0.9 firmware
... program such as HyperTerminal, and configure the selected port for: 57600 bps, 8 data bits, no ... and no flow control .
Alert Actions for NetBotz Version 2 and 3 Appliances
Control Pod or third party intelligent power strip Play Audio ... attached external, power speakers Call Web ... Sends customer alert information via the Web ... remote system Properly configured web server running ...
Video: Troubleshooting no communication between UPS and PowerChute Business Edition
Troubleshooting Windows Serial Communications for more information .
General functions of a DG5.0 control platform
... DG5.0 control platform Data Center Cooling ... : Path: Config >> Enter ... ... button >> Config . ... Press Special and Config at the same ... ... … when the Config screen comes up ... screen reads Cycle Power >> Please cycle power at the breaker ... ... Clock Card ( settings can be found ... - Power on the unit - Configure the I/ ... ... to dip switch settings which is found ... - When the Config screen comes up choose the AC Unit - Press Enter and scroll through the I/O Setup until the screen reads Cycle Power . - Please cycle power at the breaker of the unit
UPS Network Management Card 2 (NMC2) Certain Events do not work properly with the Dry Contact I/O Accessory (ap9810) Control Policy
... is able to configure these events to ... ... interface, the Control Policy Configuration is under UPS ... >sub heading Control Policy. ... interface, the Control Policy Configuration is under Configuration ->Universal ... O-> Control Policy. ... an output relay configuration because they do ... ... to an input power problem ... longer on battery power ... to an input power problem ... longer on battery power technically. More information on clearing events is available in . ... The current design does not support control policies for events which do not have a clearing event.
Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003
How to Configuring the Native Serial ... ... to find the power options applet inside control panel. ... on Start > Settings > Control Panel > Power Options ... on Start > Control Panel > Power Options (note ... to see the power options applet. ... Once inside Power Options, 4 ... on the system configuration . ... UPS tab to configure Windows to communicate ... ... NOT used to configure an APC USB ... Once configured , the UPS ... ... button to begin configuration . Select American Power Conversion as a ... ... that incorrect port settings may cause communications ... ... The proper port settings are: 8 data bits
NetBotz 750 | Configuring Network Settings
Process for configuring network settings on NetBotz version ... Establish Network Settings You must configure the following TCP/IP settings before the appliance ... ... use DHCP to configure network settings automatically, or ... terminal emulator to configure network settings manually. ... to Establish Network Settings ... uses Dynamic Host Configuration Protocol (DHCP) to configure network settings . ... When you apply power to the appliance ... ... to Establish Network Settings ... ) Plug the power cord provided with ... ... the following connection parameters : Data Bits: 8 Flow Control : None The terminal settings are correct as ...
How do I retrieve logs from my Secure-UPS XP1K9NN42RCC Power management Unit?
... -UPS XP1K9NN42RCC Power management Unit? ... -UPS XP1K9NN42RCC Power management Unit maintains ... ... a PMU’s ( Power management unit) ... ... navigate the the Configuration ->Communication ... ... restart after the configuration change. Configure a static IP ... ... typically located under control panel > network ... ... enter the IP information . ... Export Logs ( data .txt, ... txt, or config .ini ... .txt and data .txt ... .txt or data .txt, ... and choose either Data ->Log ... ... can export either data .txt Link to instructions on how to download the support information from the PMU. (follow the instructions for the NMC2)
Rack PDU 2G (AP8XXX) Network Port Sharing Information
General information regarding the Network ... Rack Power Distribution General information ... to the detailed information sections below. ... status of and configure and manage up ... ... selecting the Display Settings > Display ID ... ... the Establish Network Settings section. ... instructions below before powering up any of ... ... be achieved by powering up the units ... example, before powering up any of ... ... Then, first power up the unit ... ... its screens, power on the unit ... ... ID can be configured from the the ... ... To view the power for phase 2 ... ... 3:2 power Group Control using Network Port ...
No power out from some outlets on a Smart-UPS
No power out from some ... ... defective backplates, configuration issues, or ... ... loss of output power . SMT, SMX, and SRT series Smart-UPS support switchable outlet groups that can be controlled via software or via the front panel LCD. ... From the "" Control "" menu on the UPS, you would scroll to each outlet group and choose ""TurnON - No Delay"". This will restore power to the outlets in that group. ... For additional information on the functionality of switched outlet groups on SMT/SMX units, please review


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.