Browse FAQs

What's the correct torque for the screws on the NetShelter SX vertical mounting rails and accessory rails?

Published date: 02 October 2019

Issue:
Torque for the screws is not noted in the manual. 

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:

Torque is needed to properly tighten the mounting rails or accessory rails after they're moved. 

Resolution:

Torque Specs: 32-48 IN-LBS
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.