Browse FAQs

Can a roof fan be added to a NetShelter cabinet and only be turned on during a power outage?

Published date: 25 March 2019

Issue: 
It needs to be determined if a roof fan can be set to turn on only when the power is out. 

Product Line: 
NetShelter, NetBotz, Rack Cooling

Environment: 
AR3100, AR3105, AR3107, AR3150, AR3155, AR3157, ACF501, ACF502, ACF503, ACF504, ACF505, NBRK0250

Cause: 
A customer wants to use a roof fan as backup cooling. 

Resolution:
A roof fan can be set to turn on if the power is out when the relay output of a UPS is monitored by dry contacts on a NetBotz 250. 
The NetBotz 250 can be configured to turn on/off its outlet based on any threshold (like a dry contact).
The NetBotz 250 has to be plugged into a UPS.  
The output of the NMC must be set to trigger the output relay. 



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.