Browse FAQs

Why isn't my DNS change saving in StruxureWare Data Center Expert?

Published date: 22 July 2020

Issue:

Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes.

Product Line:

StruxureWare Data Center Expert

Environment:

StruxureWare Data Center Expert VM with single NIC configured

Cause:

It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers, only on a DCE VM server.

Resolution:

This issue does not occur when using SSH or a direct keyboard connection and the apcsetup configuration user.

This issue is slated to be resolved in DCE version 7.2.6
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.