Hub connected to NetBotz USB port supports only one serial device
Published date:
28 July 2020
Issue:
Two serial devices connected to a NetBotz appliance via USB hub fail to communicate.
Product Line:
NetBotz
Environment:
Advanced View
Cause:
Each USB port on a NetBotz appliance supports only one serial device. Do not use a USB hub to connect more than one serial device to a port on a NetBotz appliance.
Resolution:
Connect no more than one serial device to a USB hub connected to a NetBotz appliance.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.