What is the flow rate required for the InRow ACRD20x fluid-cooled unit?
Published date:
11 June 2020
Issue:
What is the flow rate required for the InRow ACRD20x fluid-cooled unit?
Product line:
ACRD200, ACRD201
Environment:
Data Center Cooling
Cause:
Resolution:
Each InRow ACRD20x fluid-cooled unit requires a flow rate of 10gpm within its loop. This is for a single ACRD20x piped to a single outdoor fluid cooler. The flow rates will vary for custom configurations consisting of multiple ACRD20x units to a single outdoor dry-cooler. Additional guidance on flow rates can be obtained from the Applications Engineering team.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.