Browse FAQs

What's the difference between shipping load, dynamic load and static load? Which standards are used to certify these ratings?

Published date: 03 October 2019

Issue:
Shipping, moving and loading cabinets requires the installer to know the difference between shipping load, dynamic load and static load ratings.

Product Line:
NetShelter SX
 
Environment:
All versions and serial ranges.
 
Cause:
Installers and designers need to make sure the load capacity of the cabinet is not exceeded during installation, travel or operation. 
 
Resolution:

Please see attachment for load ratings, definitions and standards. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.