Browse FAQs

Information returned for Liebert Systems when using Advanced Device Crawlers

Published date: 20 July 2020

Issue:

Information returned for Liebert Systems when using Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 appliances
Device Definition file for Liebert devices.

Cause:

Monitoring information

Resolution:

Information that is returned Liebert Systems when using Advanced Device Crawlers

The following information can be queried via Advanced Device Crawlers for a Liebert system assuming the Liebert DDF is installed.

Please note that not all information listed below is available on all Liebert models.

* Vendor
* Description
* Battery Time Remaining
* Battery Temperature
* Battery Voltage
* Battery Current
* Battery Capacity Available
* Battery Total Discharge Count
* Battery Total Accumulated Discharge Time
* Battery Amp Hours
* Battery Kilowatt Hours
* Battery Watt Hours
* Input Frequency
* Brown-outs Experienced
* Black-outs Experienced
* Transient (surge and spike) Conditions Experienced
* Number of Input Lines
* Input Line:Voltage
* Input Line:Current
* Input Line:Volt Amps
* Output Frequency
* Output Load
* Number of Output Lines
* Output Line:Voltage
* Output Line:Current
* Output Line:Volt Amps
* Output Power
* Inverter Status
* Inverter Temperature
* Nominal Output Voltage
* Nominal Input voltage
* Nominal Output Volt Amps
* Nominal Output Watts
* Nominal Output Frequency
* Nominal Input Frequency
* Nominal Output Volt Amp Rating
* Nominal Output Power Rating
* Switched Receptacle Status
* UPS Bypass Status
* Bypass Frequency
* Number of Bypass Lines
* Bypass Line:Voltage
* Bypass Line:Current
* Bypass Installed
* Multi-module UPS Count Connected to System Control Cabinet
"

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.