Browse FAQs

Can a 3rd party UPS be installed in the AR106V or AR106VI?

Published date: 23 October 2019

Issue:
It is unknown if a 3rd Party UPS can be installed into the AR106V and AR106VI. 


Product Line:
AR106V, AR106VI

Environment:
All versions and serial ranges.

Cause:
The NetShelter WX 6U Vertical cabinets have a mounting bracket for a 2U UPS. 

Resolution:

Any 3rd party UPS must be validated by the manufacturer to work with this cabinet prior to installation:  
The manufacturer must validate that the 3rd party UPS can be installed vertically. Not all batteries can install in this orientation. 
When shipping with a 3rd party UPS installed, the manufacturer must validate that the 3rd party UPS can ship installed using their rail kit(s), without disconnecting in transit. 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.