Browse FAQs

Why can I ping Galaxy VS NMC IP address but cannot access the web page

Published date: 08 November 2019

Issue:
Can ping Galaxy VS NMC IP address but cannot access the web page.


Product line:
Galaxy VS


Environment:
Galaxy VS NMC card


Cause:
SSL is enabled on the NMC in firmware 3.9.3.101


Resolution:
Must use HTTPS://IP Address to access card and click on risk notification in the browser.  After logging into the NMC you can change to non-SSL (http) by do the steps below.
 
  1. Click on Configuration menu
  2. Click on Network and then Summary
  3. Check mark Enable under HTTP
  4. Uncheck mark Enable under HTTPS
  5. Click on apply
  6. Reboot the NMC

 Due to California Senate Bill 327 this will be the standard configuration for 2020 and beyond

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.