Video: How to clean a Condensate drain line on an ACSC100 unit
Published date:
29 May 2019
Issue:
How to clean a Condensate drain on a ACSC100 unit..
Product line:
ACSC100 and ACSC101
Environment:
All Serial Numbers...
Cause:
Clog due to debris or sediment
Resolution:
See Attached video
This video will show you how to remove and clean clogged drain lines and clogged condensate pumps on an ACSC100 unit. Ensue the unit is powered off then unplug the unit from power. When using compressed air please ensure safety glasses are used. Will also need to create a seal to slightly pressurize the line.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.