New! Wireless USB Wi-Fi Device
• Flexible, simple installation
• Removal of traditional cabling
• Easy updates to the wireless network
• Flexible, simple installation
• Removal of traditional cabling
• Easy updates to the wireless network
APC Network Management Card has modified its security features to reflect the new internet connected device requirements.
Refreshed with latest technology and new features the Network Management Card 3 is here and is more powerful than ever
The 2nd generation network management card end of sales date is December 2020. There is an additional year of support for firmware updates to reflect any further security changes.
For more information regarding product support read the End-of-Life policy document.
Which Network Management Card is compatible with my device?
The compatibility chart breaks down the pairing between UPS models and Network Management Card.
Depending on your UPS model, the Network Management Card is embedded or pre-installed with purchase. Ensure your model includes the upgraded card by understanding the transition timeline.
Get the transition detailsUpon login, the top banner on the interface specifically states which card is installed. Smart-UPS with a bundled network management card packaging also explicitly calls out which card is present.