-
Considerations for Owning versus Outsourcing Data Center Physical Infrastructure
- Belge Tarihi: 15/05/2013
- Referans: SPD_VAVR-8HF8DC_EN
- Açıklama: When faced with the decision of upgrading an existing data center, building new, or leasing space in a retail colocation data center, there are both...
- Boyut: 497,6 kb
- Versiyon: V1
- Dil: İngilizce
-
Data Center Projects: Growth Model
- Belge Tarihi: 20/04/2010
- Referans: SPD_SNIS-6UJ2MQ_EN
- Açıklama: Long term data center or network room capacity planning may seem impossible in the face of evolving IT technology and business requirements...
- Boyut: 1,7 mb
- Versiyon: V1
- Dil: İngilizce
-
Making Large UPS Systems More Efficient
- Belge Tarihi: 14/02/2012
- Referans: SPD_VAVR-6LJV7V_EN
- Açıklama: As energy resources become scarcer and more expensive, electrical efficiency is becoming a more important performance factor in the specification and...
- Boyut: 501,6 kb
- Versiyon: V3
- Dil: İngilizce
-
Avoiding Costs From Oversizing Data Center and Network Room Infrastructure
- Belge Tarihi: 14/03/2012
- Referans: SPD_SADE-5TNNEP_EN
- Açıklama: The physical and power infrastructure of data centers and network rooms is typically oversized by more than 100%...
- Boyut: 592,6 kb
- Versiyon: V7
- Dil: İngilizce
-
Benefits of Limiting MV Short-Circuit Current in Large Data Centers
- Belge Tarihi: 26/09/2016
- Referans: SPD_VAVR-ADZKLK_EN
- Açıklama: Once IT load levels exceed just a few megawatts (MW) of power, moving more of the electrical distribution infrastructure to the medium voltage (MV)...
- Boyut: 827 kb
- Versiyon: V0
- Dil: İngilizce
-
Common Mode Susceptibility of Computers
- Belge Tarihi: 25/05/2012
- Referans: SPD_ASTE-5T3TSZ_EN
- Açıklama: This white paper examines and challenges the claims made in literature regarding the alleged high susceptibility of computers to common mode noise.
- Boyut: 580,5 kb
- Versiyon: V2
- Dil: İngilizce
-
Data Center VRLA Battery End-of-Life Recycling Procedures
- Belge Tarihi: 16/04/2010
- Referans: SPD_DBOY-7BQRWU_EN
- Açıklama: Contrary to popular belief, the recycling of lead-acid batteries, which are the most common batteries found in data centers, is one of the most...
- Boyut: 727,2 kb
- Versiyon: V1
- Dil: İngilizce
-
Four Steps to Determine When a Standby Generator is Needed for Small Data Centers
- Belge Tarihi: 01/04/2010
- Referans: SPD_SADE-5TNRKS_EN
- Açıklama: Small data centers and network rooms vary dramatically in regard to the amount of UPS runtime commonly deployed...
- Boyut: 584,1 kb
- Versiyon: V1
- Dil: İngilizce
-
Arc Flash Considerations for Data Center IT Space
- Belge Tarihi: 23/12/2014
- Referans: SPD_VAVR-6KGRYW_EN
- Açıklama: Do IT administrators violate arc flash requirements when they turn off or reset a branch circuit breaker? What about swapping out a rack power strip?...
- Boyut: 293,6 kb
- Versiyon: V0
- Dil: İngilizce
-
Modular Systems: The Evolution of Reliability
- Belge Tarihi: 16/04/2010
- Referans: SPD_SNIS-66ZTJB_EN
- Açıklama: Nature proved early on that in complex systems, modular designs are the ones that survive and thrive...
- Boyut: 522,8 kb
- Versiyon: V1
- Dil: İngilizce
prm-load-more-docs