Технические часто задаваемые вопросы



Data Center Operation | Upgrade Process
Process for obtaining the upgrade ... upgrading StruxureWare Data Center Operation . StruxureWare Data Center Operation (DCO) StruxureWare Data Center Operation (all versions ... Upgrade files for Data Center Operation are now provided ... EcoStruxure IT Help Center . ... Creating a Help Center Account & Associating ... ... Upgrading the Data Center Operation Server ... within the Help Center ... EcoStruxure IT Help Center Account & Associating ... ... into your Data Center Operation (DCO) ... ... EcoStruxure IT Help Center site, proceed ... 3 ) Log into ... ... EcoStruxure IT Help Center - Offline Product ... ... EcoStruxure IT Help Center site at: ... 3 ) Select your ...
Video: How can the Galaxy VS reduce my energy bill?
... 480v) or 10 to 50kva (208v) 3 -phase UPS for edge, small ... and medium data centers and other business- ...
Humidity Issues in IT Data Centers
Humidity Issues in IT Data Centers ... Data Center . ... There are three concerns with humidity in a data centers depending on the type of equipment in the data center ... * Tape drive operation - Humidity can dramatically affect a tape drive’s ability to read and write data. ... * Large fluctuations in humidity can cause circuit boards to expand and contract , damaging circuitry ... The default setting for NetBotz Appliances are 20-50% which may be conservative depending on the equipment in the data center .
Why does StruxureWare Data Center Expert not accept my One Time passcode?
StruxureWare Data Center Expert is not ... StruxureWare Data Center Expert ... Central / Data Center Expert all versions ... SturuxureWare Data Center Expert requires a ... and the Data Center Expert's MAC address ... 3 . If you ... ... = StruxureWare Data Center Expert Basic ... = StruxureWare Data Center Expert Standard ... = StruxureWare Data Center Expert Enterprise ... = StruxureWare Data Center Expert Virtual Machine ... = StruxureWare Data Center Operation ... call this asset for viewing purposes on ... D. Serial number is located on the top front of a hardware DCE server and in help and about in a VM or Data Center Operation . ... 10 .
What are your condenser clearances and placement requirements?
Data Center Cooling ... is the provision for a supply of ... ... which cause poor operation and possible eventual ... ... should be retained for recommendations. Height Requirement ... be at least 10 feet above the ... Walls or Obstructions For proper air flow ... ... room is left for maintenance work through ... When the unit is in an area where it is enclosed by three walls the unit must be installed as indicated for units in a pit. ... Multiple Units For units placed side by side, the minimum distance between units is the width of the largest unit. ... Decorative Fences If these requirements are not met, unit must be installed as indicated for “Units in pits”.
Data Center Operation | How to download the desktop client?
Process for downloading the Data Center Operation desktop client. ... StruxureWare Data Center Operation (DCO) ... StruxureWare Data Center Operation (DCO) ... Data Center Operation 8.X ... 3 ) Click on Download. ... Data Center Operation 7.X and earlier:
What are your humidifier specifications and control operations for the InRow RP?
What are your humidifier specifications and control operations for the InRow RP? ... Data Center Cooling ... The humidifier produces up to 6.6 lb ( 3 kg) of steam per hour. ... Humidity readings and setpoints are shown in %RH but are converted to dewpoint internally for control. ... The output for humidification is determined by the difference between the humidify setpoint and the average return air humidity of all the units in the cooling group (if more than one unit is present).
Data Center Operation | Managing Virtual Sensors
Process for managing virtual sensors in StruxureWare Data Center Expert ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (all versions) ... Virtual Sensors Limits are defined within the release notes of Data Center Expert: ... 2) Select the type of operation you want to create, either Average or Total. 3 ) Select the type of sensor you want the virtual sensor to be based off of. ... Multiple Sensors can be selected using the CTRL+Click or SHIFT+Click operations . ... 3 ) Select Device(s). ... 3 ) Confirm to Delete by clicking OK.
Data Center Expert | How do hardware and software support contracts work?
... and software support contracts work for StruxureWare Data Center Expert. StruxureWare Data Center Expert (DCE ... StruxureWare Data Center Expert (all ... Software Support Contract StruxureWare Data Center Expert appliances come ... The Data Center Expert appliance and ... Software support contracts are required for the server which ... ... currently require support contracts . Hardware Support Contracts StruxureWare Data Center Expert Appliances can ... ... must be continuous for the duration of ... Year 3 ... 7G4G48_R 3 _EN. ... Software Support Contracts ... can be provided for trail installation of ... ... not be purchased for a virtual appliance ...
Data Center Operation | Video: Copying files from the StruxureWare Data Center Operation
How to copy files from the StruxureWare Data Center Operation ... StruxureWare Data Center Operation ... StruxureWare Data Center Operation (All Versions) ... Files such as backup and logs can be "downloaded" from the Operation server using SFTP/FTP. ... Please see the instructions below for a step by step guide for "downloading" files from the server via WinSCP. ... 3 . Enter log in credentials in both "Username" and "Password" fields ... 3 . Locate the backup to save off server


Результаты 1 - 10 of 79

Не нашли то, что искали?

Обратитесь к нашей команде по обслуживанию клиентов для получения информации о технической поддержке, помощи в составлении претензий и другого.