Browse FAQs

Why is my Mac OS not a supported system for PowerChute Personal Edition v3.1?

Published date: 20 March 2020

Issue:
Mac OS is not a supported Operating System

Product Line/s:
Back-UPS
PowerChute Personal Edition

Environment:
Mac OS X attached to APC Back-UPS via USB cable

Cause:
PowerChute Personal Edition software provides safe system shutdown in the event of an extended power outage and provides potential data corruptions. Mac OS has this option available natively.

Solution:
Configure native Energy Saver options available in System Preferences. Please review FAQ FA159690 for assistance with Energy Saver options. 


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.