Browse FAQs



Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel ) is set to synchronize time.
Does the NTP need to be configured on all NMCs for all parallel Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel ) is set to synchronize time.
PowerChute Network Shutdown reports "Available runtime has been exceeded".
... event actions are carried out even if it occurs on a single UPS in a Redundant or Parallel UPS configuration .
Symmetra PX 250/500; AP9635; Flood of RTC Time adjusted values in the logs
46934 Info IM internal memory for storing configuration settings is OK IO enclosure level ... Info RTC Time adjusted value Parallel UPS 1 2 02- ...
How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?
How do I connect a EPO circuit to Smart- UPS VT or Galaxy 3500 Battery XR Frame? ... Smart- UPS VT & Galaxy 3500 Battery XR frames ... How do I connect a EPO circuit to Smart- UPS VT or Galaxy 3500 Battery XR Frame? ... This means that you shall connect UPS and XR in parallel by applying +24V on both connectors UPS j108 & XR j203, if you will EPO them both at same time. ... UPS can be configured in three other ways, concerning EPO. See UPS Installation manual for details.
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
Smart- UPS ... the use of Parallel Kit(srcpk001 ... ... A: The Parallel Kit allows you ... ... equally but if one fails (either ... , the other UPS will take over ... ... information of the UPS operation condition such ... ... addition to the 1 + 1 Parallel redundancy system, ... ... to take a UPS out of operation ... to bypass the UPS without taking their ... ... , isolating the UPS and connected equipment ... step-down transformers are used to convert a higher input voltage to a lower output voltage which might be more fitting for certain environments or system configurations .
Matrix-UPS frequently asked questions regarding installation, operation, and standards
... about the Matrix UPS ? Matrix UPS ... of a Matrix UPS . ... the APC Matrix UPS . 1 . Matrix- UPS should be set ... ... to Matrix- UPS . ... , Matrix- UPS Input Select Tap ... ... Set Matrix- UPS EU (Electronics ... of Matrix- UPS IU (Isolation ... ... of Matrix- UPS or by its ... ... from EU's " batt com" input ... ... of Matrix- UPS IU to " ... ... current Matrix- UPS settings . ... to menu " UPS Tests" and ... Matrix- UPS Noises ... The Matrix- UPS will make certain ... 1 . Loud Hum ...
Default administrator authentication phrase used by PowerChute Network Shutdown to communicate with the Network Management Card
If you are using a Redundant Smart- UPS , Multiple Symmetra, or a Parallel UPS configuration , all of the NMC authentication phrases ...
Why is my equipment dropped or rebooted while connected to my Smart-UPS?
... to Smart- UPS drops or reboots ... Smart- UPS ... a Smart- UPS can be dropped ... 1 ) - A UPS with a weak ... ... Every Smart- UPS has a " ... ... failure which the UPS self test may ... ... result in unexpected UPS behavior including load drops and the UPS turning off: - Each UPS is limited in ... ... number of the UPS tells you the ... ... determine if your UPS is capable of ... please use our UPS Selector Tool at ... plugged into the UPS , but the ... . If the UPS and surge strip ... A single piece of equipment ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.