Technical FAQs

Ask a Question

Video: Where can I download the StruxureWare Data Center Expert client software?

Issue:
Where can I download the StruxureWare Data Center Expert client software?

Product Line:
Struxureware Data Center Expert (DCE)

Environment:
Struxureware Data Center Expert (version 7.x and earlier)

Cause:
In order to discover devices and do most of the configuration required for DCE, you need to download and install the client application to your local system.


Resolution:



1) Open the DCE Appliance web interface by entering the IP address or hostname in a web browser.

2) In the upper-right corner will be an option to Download Client.
NOTE: In older versions, it may be on a different area of the web interface.

3) To continue you will need to Read and Agree to the license agreement.

4) You can now download the appliance and install it.
NOTE: See the release notes on https://help.se-dmaas.com for a list of supported operating system.


Downloading the most recent client before upgrading
The most recent versin of the Data Center Expert Desktop Client can be downloaded from the following IP, using the instructions listed above: http://159.215.66.15
NOTE: The latest version may not be immediately available on the server listed above.
Was this helpful?
What can we do to improve the information ?