Consulter la FAQ

Video: SRT UPS reports Battery Charger Event, Event Code 142

Date de publication : 27 August 2020

Issue:
The UPS reports: Battery Charger Event – event code 142 on the display or in the NMC event logs


 
Product Line:
SRT Models
 
Cause:
This event may be caused by a blown charger fuse, or bad batteries.
 
Resolution:
To determine the cause of this behavior, perform the following troubleshooting steps:
  • With the UPS input connected to AC mains, disconnect all the batteries in the system: all internal batteries and any external batteries, if used.
  • Go to the Status section on the display and under Battery, check Voltage.
Note: You do not need to perform measurements on the UPS battery terminals.
  • If the voltage displayed on the UPS display is below the “Voltage level” (refer to the below values), the charger fuse is blown and the UPS requires replacement.
  • If the voltage displayed on the UPS display is at, or above, the “Voltage level, the batteries need to be replaced.
 
Models Voltage level
SRT Li-Ion 1-1.5kVA If under 48V, the UPS shoudl be replaced.
SRT Li-Ion 2.2-3kVA If under 48V, the UPS should be replaced.
SRT 2.2kVA models If under 80V, the UPS should be replaced;
 
SRT 3kVA models If under 100V, the UPS should be replaced;
 
SRT 5-6kVA models If under 200V, the UPS should be replaced;
 
SRT 8-10kVA models If under 200V, the UPS should be replaced;
 

 

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.