Consulter la FAQ

Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)

Date de publication : 17 August 2016


Issue

Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2). 


Product Line
  • UPS Network Management Card 2 - AP9635/AP9635CH


Environment
  • Data centers with products that use AP9635/AP9635CH Network Management Card 2 (NMC2)
  • Firmware applications that support Modbus TCP or Modbus RTU with AP9635/AP9635CH (Galaxy VM, Galaxy 300/7000, Galaxy 5000/5500, etc)


Cause

This application note explains how to install the Modbus wiring for an AP9635/AP9635CH Network Management Card 2, gives an overview of the Modbus protocol, describes the Modbus packet structure, and explains how to identify and resolve common problems.

(​The Modbus protocol uses TCP, RTU and ASCII modes of transmission. The AP9635/AP9635CH supports Modbus/TCP and Modbus/RTU protocols.)


Resolution
The latest version of the Modbus Installation and Troubleshooting for AP9635/AP9635CH Management Card Application Note 168 attached below.
 

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.