Consulter la FAQ

Can I mix C10, C69 with V66 batteries in a Symmetra PX battery frames?

Date de publication : 10 June 2020

Issue:

Can I mix C10, C69 with V66 batteries in a Symmetra PX battery frames?

 

Product line:

Symmetra PX1 & PX2

 

Environment:

All models/ Serial number

 

Cause:

APC By Schneider uses multiple vendors to supply the batteries for use in Symmetra PX products. When installing the batteries into the frame they need to be installed in a specific configuration.

 

Resolution:

If batteries in columns (A and B or C and D) are of two different types, a “mixed battery” fault is generated. You may have two different vendors on the same shelf (level) as long as A&B is the same and C&D are the same. Both the Battery modules and shipping material/packaging are marked with stickers identifying the manufacturer of the batteries. This allows for installing the batteries in such a way as to not generate alarm.

 

Some common manufacturer of the batteries sticker are; C10, C69, and V66

 


Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.