Consulter la FAQ



Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Issue: Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
Cause: Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
Shutting Down the MGE Galaxy 5000 UPS ... Galaxy 5000, Galaxy 5500 ... Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS ... This procedure is for a single UPS without an external bypass panel. ... Step 1 : Touch any button on the display to wake it up. ... Step 6: Turn the Q 1 Switch to Off
Galaxy VM; Battery Electrolyte Values for Modular battery Cabinets
Galaxy VM ... The link to the web page http://www.apcmedia.com/salestools/MBPN-9M5H2Q/MBPN-9M5H2Q_R 1 _EN.pdf?sdirect=true
Galaxy 5000; Modbus Q1 Input Breaker status does not change state
The 66061 JBUS/Modbus manual was updated May 2018 to reflect the correct Modbus register for NAM Galaxy 5000 Q 1 Breaker status.
Which SmartSlot accessories are supported by the Galaxy 3500 (g3500) UPS?
... supported by the Galaxy 3500 (g3500 ... MGE Galaxy 3500 models ... supported by the Galaxy 3500 UPS ( ... The can also used with the AP9631 Network Management Card 2 to have dry contact functionality - (2) inputs, ( 1 ) output per ap9810 with a maximum of (2) ap9810 that can be attached. ... AP9622 product page ... 1 .) Purchase a right angle DB25 Male-Female interconnection ... 2.) Utilize an APC ap9600 single slot SmartSlot expansion chassis and extend the cable to the ap9600 with a 940-1500 serial cable.
Galaxy VM Seismic Certification and Anchoring Requirements.
Galaxy VM Seismic Certification ... Galaxy VM ... for documentation regarding Galaxy VM Seismic Certification ... ... to installation and site preparation work. ... the Schneider Electric website . Galaxy VM Product Home ... ... -ups/ galaxy -vm/ ... Galaxy VM- 2012 ... Galaxy VM OSHPD pre ... ... -SA- Galaxy VM Typical Seismic ... https://www.schneider-electric.com/en/download/document/APC_BYSN-9GN8T9_R 1 _EN/ Galaxy VM Installation Manual: ... Galaxy VM Seismic Anchoring Document: BYSN-9GN8T9_R 1 _EN Galaxy VM Seismic Certification Document: COCR-9X4HHB_R0_EN
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW The 66061 JBUS/Modbus card is configured for 9600, 8, N and 1 . Slave address is 1 and wiring is 2-wire with no parity and termination. This assumes only one 66061 card or UPS or STS is connected to the enclosure but if more than one change as required. ... The IP address needs to be configured at the site . ... One is down (off position) and all others are up.


Résultats 1 - 10 de 50

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.