Consulter la FAQ



Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
APC provides a 1-year warranty on each RBC. APC supplies the appropriate instructions, wires and connectors.
Why does only one fan spin on my APC step down transformer (part numbers AP9626/27/28, SYTF2, SRT5KTF, SRT5KRMTF)?
APC step down transformers come with two fans installed. One is the primary AC fan that is used for forced air cooling of the transformer.
Video: What does the Site Wiring Fault Indicator LED on my APC UPS or Surge Arrestor represent?
All 120v APC Back-UPS ... ... LED light is only present on 120v ... On APC UPS products this ... APC recommends that you ... ... >5 Volts AC measured between Neutral ... ... outlet that the APC UPS unit is ... Therefore, in order to maintain your warranty and protection under APC's Equipment Protection Policy, be sure that the APC unit is only plugged into a properly grounded outlet where the Site Wiring Fault Indicator (SWF) light is not illuminated.
What are the basic troubleshooting steps for the APC AV J-Type J25B / J35B Power Conditioner and Battery Backup?
... steps for the APC AV J- ... APC AV J- ... ... find the your APC AV J- ... ... power during a AC power outage. ... into a SURGE ONLY outlet. ... from the SURGE ONLY outlet and re ... ... while connected to AC power. ... no longer receiving AC power, or ... Ensure that the wall outlet is receiving AC power by checking it with another device. ... The AC input voltage is out of range, the frequency is out of range, or the waveform is distorted. ... Disconnect non-essential equipment from the Battery Backup outlets and connect the equipment to SURGE ONLY outlets.
Video: Configuring clearing events with APC Network Management Cards
event in the Informational event list but a recipient is only set to receive critical events, an end user will receive the Critical - UPS: On battery due to an input power problem ... notification. They may think that the UPS is still on battery and will take any appropriate actions necessary for an extended on battery event.
Can I plug my APC Rack-Mount Power Distribution Unit (Rack PDU) into a feed receptacle located in the under floor plenum? (Also applicable to Configurable & Modular Power Distribution)
645.5 Supply Circuits and Interconnecting Cables (1) The raised floor is of suitable construction, and the area under the floor is accessible. ... MC cable, or Type AC cable. ... hall be listed as Type DP. Type DP cable having adequate fire resistant characteristics suitable for use under raised floors of an information technology equipment room.
What is the battery type and technology used in APC UPS Systems?
What is the battery type and technology used in APC UPS Systems? ... All APC Single Phase UPS Battery systems. ... All APC Single Phase UPS Battery systems. ... APC UPS Systems use Valve Regulated Lead Acid (VRLA) batteries. VRLA batteries are designed to recombine hydrogen and oxygen and emit only extremely small amounts of hydrogen under normal operating conditions. ... Spill containment with VRLA batteries is therefore not meaningful or appropriate .
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
... working with an APC Network Management Card ... ... ON for your APC NMC device to ... 4.) Under Advanced, ensure you specify SMTP authentication encryption, if required, as well as the appropriate port number (both provided by your email provider). If ... and choose the appropriate recipient to test. ... The Network Management Card does this one time only per email request. ... TLS v1.1/1.2 is supported only on firmware revision v6.5.0+.
How do I mass configure APC user settings using Data Center Expert?
... I mass configure APC user settings using ... APC Network Management Cards ... APC Network Management Cards ... ... - Read- Only Password ... device and select APC SNMP Device Configuration ... menu and select APC SNMP Device Configuration ... For best results, set the protocol to FTP Only in the Device File Transfer Settings. ... This method should work on APC OS version 6.0.0 and higher, excluding v6.0.6 through v6.1.1. ... 3) Ensure to select the appropriate IP range, username, password, and protocol type for the device connection.
Video: Data Center Expert | How do I mass configure APC devices?
... for mass configuring APC devices using StruxureWare ... APC Network Management Cards ... ... device and select APC SNMP Device Configuration ... menu and select APC SNMP Device Configuration ... You will only be prompted to ... Only select the individual ... select APC SNMP Device Configuration ... You will only be prompted to ... Only existing items in ... select APC SNMP Device Configuration ... You will only be prompted to ... Only existing items in ... ... device and select APC SNMP Device Configuration ... menu and select APC SNMP Device Configuration ... You will only be prompted to ... ... online, the appropriate file transfer protocol ... ... not have the appropriate file transfer protocol ...


Résultats 1 - 10 de 77

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.