Browse FAQs



General functions of a MicroAC control platform DG3
... an electronic control for the complete management of precision air-conditioners , both in direct expansion versions (with 1 or 2 compressors ) ...
How to navigate through an Network Air FM unit display
... NetworkAIR FM DX Precision Air Conditioner . Direct expansion (DX) ... ... capacity uses one compressor and half of ... ... coil and both compressors . ... All refrigerant is directed through the expansion valve which feeds ... ... in which the compressors are engaged to ... hours that each compressor runs. ... in which the compressors are engaged. ... in which the compressors are engaged should ... ... used in the direct expansion refrigeration system. ... ... begins when the compressor engages and then prevents the compressor from disengaging until ... ... It protects the compressors from rapidly cycling ... ... can shorten the compressor life by causing ...
What is meant by ‘flooding’ with Air Conditioners?
All A/C Units with Compressors . ... Flooding (also known as ‘flood back’) is the term used to describe the condition when Liquid refrigerant reaches the compressor . ... Flood back of refrigerant to the compressor (low superheat) is defined as liquid refrigerant reaching the compressor . ... • Evaporator fans not operating.
acpa4000 Spare Parts List
234-4206 CAP MTL PPR 45UF 10% 370vac ( compressor ... 0p4582 COMPRESSOR ROTARY 115/1/60 (PANASONIC style compressor ... 0M-6326A Condensate Pump EC -400 Little Giant (yk0501 below ... 0M-2470 Condenser Fan ( fan only 490-1045 Condenser Fan Box Sub Assy ( fan housing assy ... 870-3663 Evaporator Fan Box Assy ( fan only 490-1046 Evaporator Fan Box Sub Assy ( fan w/ housing assy ... 540-0088 Switch Thermal Overload Protector (for compressor pecker head
Where can I get support for APC and MGE Products?
AC Power ... InRoom Direct Expansion ... InRow Direct Expansion ... Operations Energy Efficiency ... SmartSlot Expansion Chassis
Refrigerant charging table for a Uniflair Unit
... be short and direct as possible. ... proper refrigeration/ AC vibration clamps. ... return to the compressor . ... ) of the compressor to ensure that ... ... back to the compressor during shutdown Liquid lines must be sized to ensure sufficient refrigerant flow to the expansion device and to minimize pressure drop. ... 5. Start the compressor , and complete the charging process. ... to avoid compressor damage.
APC Schneider Cooling Unit Identification
E= Expansion A= Air Cooled ... Compressor ... E= Fan Coil/Evap BC=208/1/60 ... R= Remote X= No Compressor 2= With Compressor S= Spot Cooled ... IC= Indoor Centrifugal C= Fan Cycle F= Fan Speed ... AFS= Air Cooled Fan Speed Control ... DX= Direct Expansion ... Compressor
What are the operational conditions for an InRoom (Stulz) Unit
Resolution: The InRoom precision air conditioning units operate within the following ranges:
Why does only one fan spin on my APC step down transformer (part numbers AP9626/27/28, SYTF2, SRT5KTF, SRT5KRMTF)?
APC step down transformers come with two fans installed. One is the primary AC fan that is used for forced air cooling of the transformer.
Can I operate my A/C in ambient temperatures below 65f
Product line: All compressor ac units


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.