Browse FAQs



Where can I get support for APC and MGE Products?
Universal Mobile Device Batteries Universal Notebook Batteries
Configuring Microsoft Vista, Windows 7, 8, & 10, Windows 2008 & 2012 to safely shutdown without using APC's PowerChute software.
Once a USB UPS is connected, the OS adds configuration similar to that of a laptop with an on-board battery .
Troubleshooting steps to perform when "Please check that the USB cable between your battery backup and PC is properly connected" message or "Unknown Device" appears after a reboot of your computer.
... cable between your battery backup and PC ... ... with the following APC Battery Back-UPS ... ... the left of Universal Serial Bus Controllers ... ... properly recognized the APC UPS correctly. ... see listings as Batteries and Human Interface ... ... cable between your battery backup and PC ... If so, there are a few parameters of your PCs BIOS that need to be changed in order for your PC to recognize the USB device as an APC UPS after each boot. ... Note: An APC representative cannot make changes or assist customers in making changes to the BIOS, as it is a liability to APC .
Back-UPS is detected as an ""Unknown Device"" in Device Manger
All APC Back-UPS ... All APC Back-UPS ... ... the installation of APC's Power Management Extensions ... ... the installation of APC's Power Management Extensions ... , "" Universal Serial Bus controllers ... XXX "" Universal Host Controller" ... ... cable between your battery backup and PC ... ... device as an APC UPS after each ... ... Note: An APC representative cannot make ... a liability to APC . ... , please contact APC's Technical Support in ... ... please refer to APC's worldwide contact page ... APC has developed a ... APC strongly recommends the use of this special connector with Compaq 5000/5100/5200 series computers.
Video: Universal Transfer Switch; Fuse Removal and Manual Circuit Bypass.
Issue: APC Universal Transfer Switch; Fuse Removal and Manual Circuit Bypass.
How do I recycle APC batteries in the US and Canada?
Issue: How do I recycle APC batteries in the US and Canada?
What is the expected life of my APC UPS battery?
Most APC batteries should last three to five years. There are many factors which affect Battery life including environment and number of discharges.


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.