Technical FAQs

Ask a Question

NetBotz 4.1 IP filter features help.

Issue:

NetBotz 4.1 new IP filter features help

Product Line:

NetBotz

Environment:

NetBotz version 3 appliances
4.1 botzware

Cause:
Help with the functionality of the IP filter feature on NetBotz.

Resolution:

The attached file outlines the newer functionality of the IP filter feature on NetBotz. The document outlines adding new filters, expanding filter features, configuring the filters, as well as some example configurations
 
Was this helpful?
What can we do to improve the information ?