Últimas Novidades/ComunicadosRecursos MediaDocumentaçãoHiperligações rápidas |
New Schneider Electric Smart-UPS On-Line Are First Single-Phase Range With Unity Power Factor Capability
London, 10th June 2014: Schneider Electric, a leader in energy management and critical power supplies, has announced its new 5 – 10kVA APC by Schneider Electric Smart-UPS On-Line UPS range. The 6 – 10kVA units are the company’s first single-phase UPS range to feature unity power factor capability, while the 5kVA UPS have 0.9 power factor.
Bill Manning, VP Business Power Solutions, Schneider Electric said, “With rising cost of energy and concerns over efficiency, IT and facility professionals are keen to minimise waste by ensuring a better fit between infrastructure and load requirements. Our unity power factor UPS help reduce waste as well as complexity when specifying power protection. Unity power factor provides more real power for the active power factor corrected Switched Mode Power Supplies typically found in most IT servers and network equipment.”
The new Smart-UPS On-Line offers efficient power quality and performance in a compact footprint. Its flexible design allows the units to be configured for rack-mounted or free standing applications, making the new UPS easy to install, operate and service in almost any environment. The range is complete with an embedded network management card enabling further accessories and communication options to be conveniently added.
Ideal for a range of applications, from network and server rooms to branch offices and secure power uses, the new APC Smart-UPS On-Line utilise double conversion, on-line topology. This high availability design, in which the inverter continuously provides regulated power output, means the UPS can be used to protect equipment that is not resilient to the slightest break in voltage or variations in frequency (e.g., devices with linear power supplies which are ubiquitous in the process and control industries).
However, since most computer and networking equipment can easily ride through small voltage breaks (>20ms), Smart-UPS On-Line can also be operated in a high efficiency operating “green” mode. In a steady state, double conversion operations are bypassed to enable up to 97% UPS efficiency*. Not only does this reduce power use and cost, but also the cooling required as units create fewer heat losses. Lower heat also leads to longer life of key components such as batteries.
A graphical LCD with multi-colour backlight provides a real-time, at-a-glance display of UPS status. The LCD also provides diagnostic and log information that that may be helpful to identify power issues before they result in any downtime. To enhance efficient operations and energy monitoring, the units also feature a built-in Energy Meter.
The new Smart-UPS On-Line range also features Intelligent Battery Management with Predictive Battery Replacement that continually adjusts to enhance battery life, enables users to check the health of each battery (including those in external packs) and provides the most advanced warning that a battery needs to be replaced. In the event of a failure, a user interface enables the specific battery to be easily located and recommends if the user should replace other batteries at the same time. Batteries are hot-swappable and can be replaced with no interruption to operations.
The new range has been designed with a fast recharge time, providing high uptime in installations where chronic power problems may result in multiple successive power outages within a short period of time. Additionally, the UPS can operate with or without a charged battery to guarantee load restart once utility power is restored.
For confidence and peace of mind, the new Smart-UPS On-Line UPS are complete with a three-year warranty. To get more details, please visit www.schneider-electric.com and www.apc.com
==Ends==
About Schneider Electric As a global specialist in energy management with operations in more than 100 countries, Schneider Electric offers integrated solutions across multiple market segments, including leadership positions in Utilities & Infrastructure, Industries & Machines Manufacturers, Non-residential Building, Data Centres & Networks and in Residential. Focused on making energy safe, reliable, efficient, productive and green, the Group’s 150,000 plus employees achieved sales of 24 billion euros in 2013, through an active commitment to help individuals and organizations make the most of their energy.
www.schneider-electric.com
Editor’s Note *Whilst in “green” mode, should the quality of the utility supply drop outside of configurable ranges the UPS will immediately and automatically switch back into on-line mode in less than 10ms.
For more information contact: Web: www.apc.com
Press enquiries: Email: dwells@spacomms.co.uk
Contactos RP APC Hill & Knowlton
Contato: Carlos Duarte
Telefone: +351 21 413 62 00
|