A sealed IT enclosure to build up a Micro Data Center solution for industrial use and commercial applications which require dust and water protection. Designed for the integration of IT equipment and physical infrastructure components.
AR5340
A sealed IT enclosure to build up a Micro Data Center solution for industrial use and commercial applications which require dust and water protection. Designed for the integration of IT equipment and physical infrastructure components.
A sealed IT enclosure with ventilation system to build up a Micro Data Center solution for industrial use and commercial applications which require dust and water protection. Designed for the integration of IT equipment and physical infrastructure components.
AR5340F
A sealed IT enclosure with ventilation system to build up a Micro Data Center solution for industrial use and commercial applications which require dust and water protection. Designed for the integration of IT equipment and physical infrastructure components.
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
NSYSFRSEDC2812E
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
NSYSFRSEDC281E
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
NSYSFRSEDC268E
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
NSYSFRSEDC261E
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
NSYSFRSEDC1268E
IP 55 rated assembled enclosure for OT, IT and networking applications. Form factor to easily roll through doorways. Configurable to work as a ventilated enclosure with the addition of IP54 Climasys ventilation components. Includes: Front and rear solid doors with handle and insert key, side panels, 19" uprights, bottom plinth, grounding and gland plate at the bottom panel. Ventilation system not included. Can be shipped pre-integrated with UPS, PDU, monitoring components and internal equipment up to 158 kgs
IT enclosures designed for specific environments and applications
Rack system components that can be added to existing racks if requirements change.
AR8354
Rack system components that can be added to existing racks if requirements change.
Rack system components that can be added to existing racks if requirements change.
AR8353
Rack system components that can be added to existing racks if requirements change.
Rack system components that can be added to existing racks if requirements change.
AR8350
Rack system components that can be added to existing racks if requirements change.
Rack system components that can be added to existing racks if requirements change.
AR8352
Rack system components that can be added to existing racks if requirements change.
Rack system components that can be added to existing racks if requirements change.
AR8351
Rack system components that can be added to existing racks if requirements change.
Rack system components that can be added to existing racks if requirements change.
AR8352X342
Rack system components that can be added to existing racks if requirements change.
Stabilization plates to prevent tip-over in stand-alone rack applications.
AR8111
Stabilization plates to prevent tip-over in stand-alone rack applications.
Rack system components that can be added to existing racks if requirements change.
AR8130BLK
Rack system components that can be added to existing racks if requirements change.
Premium solution for a secure, managed network environment
AR1001AX182
Premium solution for a secure, managed network environment
Premium solution for a secure, managed network environment
AR1001A
Premium solution for a secure, managed network environment
Netshelter CX Enclosure with integrated cooling and noise dampening is ideal for office environments. The cabinet is paired with a shock absorbing pallet, unloading ramp and impact resistant shell. The system has been engineered, tested and approved for secure shipment of fully integrated IT systems
AR4038SPX431
Netshelter CX Enclosure with integrated cooling and noise dampening is ideal for office environments. The cabinet is paired with a shock absorbing pallet, unloading ramp and impact resistant shell. The system has been engineered, tested and approved for secure shipment of fully integrated IT systems
Netshelter CX Enclosure with integrated cooling and noise dampening is ideal for office environments. The cabinet is paired with a shock absorbing pallet, unloading ramp and impact resistant shell. The system has been engineered, tested and approved for secure shipment of fully integrated IT systems
AR4038SPX429
Netshelter CX Enclosure with integrated cooling and noise dampening is ideal for office environments. The cabinet is paired with a shock absorbing pallet, unloading ramp and impact resistant shell. The system has been engineered, tested and approved for secure shipment of fully integrated IT systems
Netshelter CX Enclosure with integrated cooling and noise dampening is ideal for office environments. The cabinet is paired with a shock absorbing pallet, unloading ramp and impact resistant shell. The system has been engineered, tested and approved for secure shipment of fully integrated IT systems
AR4038SPX432
Netshelter CX Enclosure with integrated cooling and noise dampening is ideal for office environments. The cabinet is paired with a shock absorbing pallet, unloading ramp and impact resistant shell. The system has been engineered, tested and approved for secure shipment of fully integrated IT systems
Netshelter CX Enclosure with integrated cooling and noise dampening is ideal for office environments. The cabinet is paired with a shock absorbing pallet, unloading ramp and impact resistant shell. The system has been engineered, tested and approved for secure shipment of fully integrated IT systems
AR4038SP
Netshelter CX Enclosure with integrated cooling and noise dampening is ideal for office environments. The cabinet is paired with a shock absorbing pallet, unloading ramp and impact resistant shell. The system has been engineered, tested and approved for secure shipment of fully integrated IT systems
Wizards, Configurators and Utilities for network managed devices.
SDW30
Wizards, Configurators and Utilities for network managed devices.
Rack enclosures with advanced cooling, power distribution, and cable management for server and networking applications in IT environments.
AR2100BLKX425
Rack enclosures with advanced cooling, power distribution, and cable management for server and networking applications in IT environments.
Open rack system for easy access to IT equipment and cabling.
AR203A
Open rack system for easy access to IT equipment and cabling.
Open rack system for easy access to IT equipment and cabling.
AR204A
Open rack system for easy access to IT equipment and cabling.
Premium solution for a secure, managed network environment
Open rack system for easy access to IT equipment and cabling.
AR201
Open rack system for easy access to IT equipment and cabling.
Wireless USB receiver and router. When plugged into compatible appliances, it enables a wireless network to be created. When used with the included power supply, it extends the range of the wireless network.
NBWC100U
Wireless USB receiver and router. When plugged into compatible appliances, it enables a wireless network to be created. When used with the included power supply, it extends the range of the wireless network.