As nossas marcas

EcoStruxure IT Advisor CFD

Nenhuma imagem do produto
Nenhuma imagem do produto
  • Visão geral imediata das operações do centro de dados através da gestão do inventário, calculadora PUE, alarmes de dispositivos em tempo real e informação detalhada ...

Veja a descrição geral do produto

SFTWCFD Características

EcoStruxure IT Advisor CFD
Visão geral imediata das operações do centro de dados através da gestão do inventário, calculadora PUE, alarmes de dispositivos em tempo real e informação detalhada (“drill-down“) baseada na locali...
  • Accuracy
    EcoStruxure IT Advisor CFD solves a full-physics version of the Navier-Stokes Equations. More importantly, ITA CFD’s pre-configured objects and 100% automatic computational grid ensure that all users, from novice to CFD expert, obtain the same consistent high accuracy.
  • Context Awareness
    Object placement is intuitive and mirrors real-world data centers. For example, containment volumes can be simply placed adjacent to IT Rack front or rear faces. Similarly, racks and cooling units can be ducted to a dropped-ceiling with a single menu selection. ITA CFD’s powerful IT Rack model automatically includes the effects of leakage airflow and recirculation inside of the rack. This means that IT Racks can be uncontained, contained, placed with their rear faces against a wall, etc. ITA CFD’s unique Cooling Check assesses cooling performance (with a graphical indication on the top of each rack) based on the type of containment that has been specified (or not). For example, the Cooling Check will provide warnings if insufficient exhaust air is captured at the rear of the rack when rear (hot-aisle) containment is configured.
  • Easy Access
    EcoStruxure IT Advisor CFD is available by subscription and runs entirely in your web browser. Nothing is installed locally and there are no hardware requirements as all CFD calculations run in the cloud.
  • Easy Model Creation
    Start a room model from scratch or use one of the many Reference Models as a starting point. Pre-configured models of common data center equipment include all required physics; they can be “stamped” into position and duplicated as desired. Equipment is intuitively placed on white space floor - then moved in the vertical direction if desired.The computational grid and other CFD settings are entirely automatically and transparent to the user.
  • Fast and Robust Analysis
    EcoStruxure IT Advisor CFD’s solver is efficiently parallelized and runs on high-end graphical processing units (GPUs) in the cloud. Not only is ITA CFD uncommonly fast among CFD tools, but it is uncommonly robust too thanks to its automatic grid cell generation and inherently-transient solution method.
  • Simple Visualization Tools
    The Cooling Check indication on each rack provides a comprehensive cooling assessment at a glance. The rack pop-up menu gives additional details about the internal-rack airflows along with External Capture Indices. The latter metrics quantify the effectiveness of the cooling architecture in delivering cool air to the rack inlet and scavenging warm air from the rack exhaust. Temperature, pressure, speed, and velocity vectors can be displayed at any 2D slice and you can use your mouse as a probe to see values at any point in the room. Raised-floor and dropped-ceiling tiles can be colored by airflow rate.

Data Center Operation Características & Benefícios

Protecção

Password security
Protecção por password escolhida pelo utilizador.
Acesso Só de Leitura
A opção só de leitura de utilizador permite partilhar o acesso sem arriscar alterações de configuração não autorizadas aos sistemas.
Acesso a múltiplos utilizadores
Permite que diversos utilizadores efectuem trabalhos na aplicação em simultâneo.
Papéis dos utilizadores
Permitir diferentes níveis de acesso através de início de sessão de utilizadores múltiplos e papéis de utilizador predefinidos.

Conveniência

Acções recomendadas
A Enterprise Manager fornece uma descrição pormenorizada dos problemas conforme estes ocorrem, bem como, as acções recomendadas que podem resolver o problema associado. Esta característica única reduz a necessidade de formação e acelera a resolução dos problemas relacionados com a energia.
Integração CAD
Permite a importação de desenhos do Desenho Assistido por Computador (CAD) de forma a remodelar rapidamente a sala e converter os desenhos da estrutura CAD no modelo, incluindo alternar as camadas CAD para mostrar toda a informação das instalações disponíveis.
Referências com base na rede
Abordagem flexível para as coordenadas do piso permitindo que os operadores do centro de dados adoptem um esquema de identificação de localização personalizada.

Gestão

Vista dianteira do bastidor
Uma vista frontal detalhada do bastidor oferece uma representação gráfica exacta do equipamento e da sua localização no bastidor.
Divisões múltiplas
Fornece a opção para apresentar múltiplas salas na mesma planta para representar e navegar com precisão em instalações grandes.
Vista organizacional
Providencia informação detalhada baseada na localização para um modelo lógico do centro de dados, onde as salas de centros de dados podem ser organizadas por regiões, países, campos universitários, locais, edifícios e salas.
Biblioteca de activos
Utiliza a extensa biblioteca de infra-estruturas físicas e dispositivos TI de fornecedores líderes.
Loja virtual
Mantém o rastro dos novos dispositivos da chegada ao local dentro da sala de armazém virtual.
Vista de disposição no piso
Visualiza a representação exacta do seu centro de dados através de visualização gráfica de disposição do chão e vista de cima.
Pesquisa global de ativos
Localiza rapidamente bens através da pesquisa livre de texto e exporta dados do equipamento para o formato excel.
Dispositivos personalizados
Personalização rápida dos dispositivos de catálogo de acordo com as suas especificações, em apenas 2 cliques, corrigindo as propriedades de personalização, tais como requisitos de energia e endereços MAC, etc.
Vista personalizável
Providencia informação detalhada baseada na localização para um modelo lógico do centro de dados, onde as salas de centros de dados podem ser organizadas por regiões, países, campos universitários, locais, edifícios e salas.

Disponibilidade

Operações em centros de dados móveis
Integra-se com o InfraStruxure Mobile para acesso à aplicação InfraStruxure Operations em movimento através do PDA de mão da Motorola (símbolo) MC70.
Calculadora PUE/DCiE
Disponibiliza o valor da Eficácia de Utilização de Energia (PUE) para informação sobre a utilização diária de energia.
Relatório de inventário
Inclui informação estruturada sobre todos os dispositivos montados em rack organizado por tipo de dispositivo, idade, fabricante e propriedades, para uma visão geral rápida de todos os dispositivos actuais dentro de um centro de dados.
Painel de instrumentos ativo
Ganha transparência para indicadores chave de desempenho do centro de dados através de painéis de controlo facilmente configurados na web, apresentando informação ao nível da gestão personalizável.
Alarmes com disposição física
Disponibiliza falhas de equipamwento em tempo real, referente ao estado de funcionamento do datacenter
Gestão de rede orientada
Uma visão geral gráfica dos percursos de rede do centro de dados e respectivas interligações.
Gestão de inventário
Mostra os dados do dispositivo dentro da disposição física, para acesso imediato aos detalhes do dispositivo e aos atributos dos activos, bem como visão geral das operações do centro de dados.
Suporte do servidor “blade”
Reproduza a configuração exacta do centro de dados por modelação de servidores "blade" dentro dos respectivos armários "blade".
Plataforma da empresa
Elevada disponibilidade com redundância de "failover" através de uma configuração agrupada e equilíbrio da carga, assegurando um sistema de missão crítica sem um ponto individual de falha.

Localização partilhada

Cliente Web
Permite ao utilizador visibilidade de ativos de centros de dados, consumo e capacidade de energia através de qualquer navegador web. Isto reduz os custos de manutenção e permite que os gestores tomem decisões em tempo real melhores e mais informadas.
Análise de impacto nos locatários
Activos da organização no mapa ao nível de uma sala, estrutura, bastidor ou servidor para um conhecimento profundo do impacto da organização no caso de um corte de energia.
Relatório do inventário de locatários
Mostra todo o equipamento associado à organização, para um inventário de organizações instantâneo.
Vista 3D da estrutura
Descreve os perímetros de estrutura para uma visualização 3D instantânea da disposição, bem como um cálculo automático da área da estrutura.
Registo de auditoria
Acompanhe todas as alterações do equipamento das instalações e da estrutura relativamente ao ciclo de vida do centro de dados, assegurando a transparência e a fácil identificação dos requisitos de manutenção.
Visualização da estrutura
Visualize o espaço disponível actualmente com dados anónimos da organização durante a fase de pré-venda para planeamento de potenciais caixas de novos clientes, reservando espaço e apoiando o processo de vendas.
Relatório da alimentação
Descreve a capacidade total vs. a capacidade de venda e a carga medida por local para uma vista geral completa das actuais capacidades de energia.
Relatório de espaço
Vista geral instantânea das capacidades do espaço actual, identificando o espaço vendável, ocupado e reservado, bem como o espaço identificado como estando a ser utilizado internamente.
Potência medida da estrutura
Permitindo um estorno detalhado a organizações individuais através de uma fácil visualização geral da energia vendida e medida.
Relatório da tomada de alimentação
Realça o estado actual de fichas e tomadas para uma ou mais PDUs ou organizações, incluindo uma indicação de subscrições excessivas.

Agilidade

Localização
Interface de utilizador disponível na maioria dos idiomas locais.
Serviços de implementação opcional
Assegurar uma rápida implementação através da utilização dos Serviços Profissionais APC.
Suporte eléctrico da sala
Monitorizar a capacidade e planificar alterações para equipamento de alimentação centralizado nas áreas exteriores da planta do centro de dados principal.
Modelo de dados partilhados
Garantir dados acabados e sincronizados ao longo de todo o ciclo de vida do centro de dados.
Independente
Permite a modelação de dados a partir de qualquer vendedor, fornecendo suporte para ambientes de centros de dados existentes.

Distribuição do produto

Emirados Árabes Unidos, Argentina, Áustria, Austrália, Bélgica, Bulgária, Brasil, Canadá, Suíça, Chile, China, Colômbia, Costa Rica, Sérvia e Montenegro, República Tcheca, Alemanha, Dinamarca, Argélia, Estônia, Egito, Espanha, Finlândia, França, Reino Unido, Grécia, Hong Kong, Região Admin. Especial da China, Croácia, Hungria, Indonésia, Irlanda, Israel, Índia, Itália, Japão, Coreia do Sul, Lituânia, Letônia, Marrocos, Macedônia, México, Malásia, Nigéria, Holanda, Noruega, Nova Zelândia, Peru, Filipinas, Polônia, Portugal, Romênia, Rússia, Arábia Saudita, Suécia, Cingapura, Eslovênia, Eslováquia, Tailândia, Tunísia, Turquia, Taiwan, Ucrânia, Estados Unidos, Vietnã, África do Sul

Opções

Serviços