Browse FAQs

What functionality does the LDAP feature provide on the NetBotz 750?

Published date: 21 July 2020

Issue:

What functionality does the LDAP feature provide on the NetBotz 750?

Product Line:

NetBotz

Environment:

NetBot version 5x rack access
LDAP / Active Directory.

Cause:

The rack access component of the NetBotz 750 includes an LDAP section.

Resolution:

When you swipe a HID card, it registers within the NetBotz device. Once LDAP is configured within the appliance, you can then associate the card with an LDAP user.
This does not pull any rights from the LDAP server but simply checks to see if the user is valid.
If the user still exists within the LDAP system, the NetBotz appliance will then check it's local settings for door access and allow or disallow access at that time.
If the LDAP user no longer exists, the NetBotz appliance will not allow access even if other door and time configuration options are configured to allow it.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.