Search FAQs
Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?
Issue:
Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?
Product Line:
NetBotz
Environment:
NetBotz cameras
Cause:
NetBotz has released the NBPD0165 camera pod.
Resolution:
No, the camera pod NBPD0165 is not compatible with NetBots 3xx, 4xx, and 5xx devices. There are currently no plans to integrate the cameras into the older appliances. As of it's release, it is only compatible with the NetBotz 750 series appliances.
Can I use a NetBotz NBPD0165 camera pod with older NetBotz appliances?
Product Line:
NetBotz
Environment:
NetBotz cameras
Cause:
NetBotz has released the NBPD0165 camera pod.
Resolution:
No, the camera pod NBPD0165 is not compatible with NetBots 3xx, 4xx, and 5xx devices. There are currently no plans to integrate the cameras into the older appliances. As of it's release, it is only compatible with the NetBotz 750 series appliances.
Released for:APC Singapore
Explore more
Explore more