Browse FAQs

Standard Lens Specifications for the WallBotz 320 & 420

Published date: 03 December 2019

Issue:

Standard Lens Specifications for the WallBotz 320 & 420

Product Line:

NetBotz

Environment:

NetBotz 320 and 420 Camera

Cause:

Standard Lens specifications.

Resolution:


* Manufacturer: Senview
* Model: TN0416F
* Size: ¼” format
* Focal Length: 4mm
o The focal length distance between the lens and the imager.
* F-Stop: 1.6
o The f-stop affects depth of field, or how much is in focus in front of and behind the subject.
* Field of View (horizontal x vertical in degrees): 48 x 37 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.