Sök bland vanliga frågor



Can the NetShelter SV be joined to a NetShelter SX?
Issue: Customers are using the NetShelter SX and SV in a row based design.
What are the differences between the NetShelter SX and SV cabinets?
Issue: Differentiate between NetShelter SX and SV cabinets.
What is the IP (Internal Protection) rating of the NetShelter SX, SV and CX cabinets?
Issue: Internal Protection (IP) rating of the NetShelter SX , SV and CX cabinets is required.
Do NetShelter SX or SV cabinets in NAM have UL stickers? If so, where are they located?
Issue: A customer needs to know if the NetShelter SX or SV cabinets have UL stickers, and where they are.
Is ISO 9001 or 14001 available for NetShelter SX, SV or CX cabinets?
Product Line: NetShelter SX , SV or CX cabinets and all accessories.
What is the maximum roof load rating for NetShelter SX and SV cabinets?
Resolution: The roofs of both the NetShelter SX and SV cabinets are rated to 200 lbs.
Are there spare or replacement keys available for the NetShelter SX, SV or VX cabinets?
This is a single spare key which works on the NetShelter SX , SV and VX doors and side panels.
Can the split rear doors of a NetShelter SX, SV or VX cabinet be installed on the front of the cabinet, and can the front door be installed on the rear?
Data center layout requires NetShelter SX , SV or VX cabinet to be flexible and allow the customer to choose what door style is installed ...


Resultat 1 - 10 av 52

Hittar du inte det du letar efter?

Kontakta vår kundtjänst för att få information om teknisk support, hjälp med klagomål och mycket mer.