{}

Our Brands

Search FAQs

Network Management Card 660674/34003640SE; Ripple20 vulnerability status

Issue:
Ripple20 vulnerability status



Product line:
660674/34003640SE Network Management Card (NMC)


Environment:
660674/34003640SE Network Management Card (NMC)


Cause:
Information about the 66074 NMC and the Ripple20 vulnerability (Treck Inc.’s embedded TCP/IP stack).


Resolution:

The 66074 NMC does not use the Treck Inc.’s embedded TCP/IP stack for TCP/IP but use a inhouse TCP/IP stack developed by the NMC vendor.  This NMC is not affected by this vulnerability.


APC Saudi Arabia

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.