Browse FAQs

Erroneous Fan alarms on the XU1K3LLXXRCC

Published date: 13 August 2020


Issue:

XU1K3LLXXRCC may report erroneous Fan alarms

Product Line:

Smart-UPS Industrial

Environment:

XU1K3LLXXRCC, All Serial Numbers, firmware less than UPS Firmware 2.5

Cause:

Earlier revisions of the UPS Firmware may report erroneous Fan alarms

Resolution:

Upgrade the unit to the latest UPS firmware

UPS Firmware 2.5 introduced improvements to fan status reporting, among other things.
Full release notes are attached to this FAQ.

To upgrade via the Network Management Card refer to FAQ #FA281753
To upgrade via a USB Thumb Drive refer to FAQ #FA402857


You can download the XU1017UPS_02-5.enc firmware image here.
Release notes are attached below.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.