{}

Our Brands

Search FAQs

How to enable .NET 2.0 on Windows 8.x and 10

Issue:
PowerChute Personal Edition 3.0.2 will not install on Windows 8 or 10 because the system in missing .Net 2.0

Product Line:
PowerChute Personal Edition 3.0.2

Environment:
Windows 8.x and 10

Cause:
.Net 2.0 is not pre-installed as part of the OS

Solution:

You will need to install the .Net 3.5

1. Open up the control panel.  (Right click start - then click control panel)

2. Verify the control panel is in Icon view

3. Go to Programs and features

4. In the left side of the window there is an option for "Turn Windows features on or off" select that.

5. You should see .NET Framework 3.5 (includes .NET 2.0 and 3.0). Check the box to the left of the .NET Framework 3.5 and click ok.  Windows will proceed to install the service (downloading it from windows update if necessary).

6. After add .Net 3.5 that includes .Net 2.0 you can now install PowerChute Personal Edition 3.0.2

APC Saudi Arabia

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.