{}

Our Brands

Search FAQs

How to Load VMware vSphere Client onto a PC

Issue:
How to Load VMware vSphere Client onto a PC

Product Line:
VMware vSphere Client

Environment:
Microsoft Windows XP, Vista, Win 7, Win8, Win8.1, Win 10
NOTE: vSphere Client requires .Net Framework 3.5 be present before it will install properly. Windows XP, 8.x, and 10.x do not ship with .Net Framework 3.5 so it must be installed prior to installing vSphere client. See Microsoft forum post http://answers.microsoft.com/en-us/windows/forum/windows8_1_pr-networking/when-installing-the-vmware-vsphere-51-client-i-get/8cfa9152-fb46-432e-99f3-3ba3558f3845 for more information.

Cause:
Informational

Solution:

Please review the attached PDF.

APC Saudi Arabia

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.