{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Netbotz 500, 420, or 320 loses configuration when it is rebooted.
Issue:
Netbotz 500, 420, or 320 loses configuration when it is rebooted
Product Line:
NetBotz
Environment:
Version 2 NetBotz
Cause:
Due to a change on the Netbotz devices, some 500s, 420s, and 320s made in mid 2007 began losing some configuration when the system was rebooted. Prior to rebooting the device, the unit would function normally.
Resolution:
Version 2.6.2 of Botzware has fixed this issue.
Netbotz 500, 420, or 320 loses configuration when it is rebooted
Product Line:
NetBotz
Environment:
Version 2 NetBotz
Cause:
Due to a change on the Netbotz devices, some 500s, 420s, and 320s made in mid 2007 began losing some configuration when the system was rebooted. Prior to rebooting the device, the unit would function normally.
Resolution:
Version 2.6.2 of Botzware has fixed this issue.
Explore more
Range:
Explore more
Range:
Can't find what you are looking for?
Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.